REC.GAP
Description
REC.GAP specifies the gap between consecutive samples. The recording base rate is 16 kHz, thus a gap of 1 means that a sample is recorded every 62.5 µs.
Example
Code
To record data every 125 us:
-->REC.GAP 2
Context
For more information see Scope.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type |
Read/Write |
Units |
N/A |
Range |
1 to 65,535 |
Default Value |
1 |
Data Type |
Integer |
See Also |
|
Stored in Non-Volatile Memory |
No |
Variants Supported
All variants are supported.
Fieldbus Information
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
---|---|---|---|---|---|---|
2302 |
1 |
2302 (0x8fe) |
REC.GAP |
Unsigned16 |
Read/Write |
Yes |
Parameter |
PNU |
Data Type |
Access |
Units |
---|---|---|---|---|
REC.GAP |
2302 |
Unsigned16 |
Read/Write |
- |